Issue:
Can I run 2 ATV320 drives separately from 1 HMI?
Product Line:
ATV320
Environment:
All
Cause:
N/A
Resolution:
This can be done with a Magelis HMI using Modbus or other Serial Communication protocol that is supported by the ATV320.
The ATV320 remote keypad or HMI can only control 1 drive at a time.
Can I run 2 ATV320 drives separately from 1 HMI?
Product Line:
ATV320
Environment:
All
Cause:
N/A
Resolution:
This can be done with a Magelis HMI using Modbus or other Serial Communication protocol that is supported by the ATV320.
The ATV320 remote keypad or HMI can only control 1 drive at a time.
Released for: Schneider Electric Egypt and North East Africa