Issue:
Is additional line reactor needed with the process drives?
Product Line:
Altivar 600
ATV630, ATV650
Altivar 900
ATV930, ATV950
Environment:
All
Resolution:
The internal DC chokes provide a impedance between about 2 and 3.5%, depending on the drive.
If higher total impedance is needed, then a line reactor can be added up to max 5% total impedance (built-in plus additional combined).
Is additional line reactor needed with the process drives?
Product Line:
Altivar 600
ATV630, ATV650
Altivar 900
ATV930, ATV950
Environment:
All
Resolution:
The internal DC chokes provide a impedance between about 2 and 3.5%, depending on the drive.
If higher total impedance is needed, then a line reactor can be added up to max 5% total impedance (built-in plus additional combined).
Released for:Schneider Electric Egypt and North East Africa