Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you program the ATV320 drives' STO safety inputs from the keypad or HMI?
Issue:
ATV320 program the STO safety inputs from the keypad or HMI.

Product Line:
ATV320

Environment:
All

Cause:
Wants to know if you can program the STO safety inputs with the local keypad or remote HMI?

Resolution:
The ATV320 drives' STO functions can only be configured using the Somove software.