M580 - Is it possible to pack the memory of an M580 HSBY PLC online in run mode?
Question:
Is it possible to pack the memory of an M580 Hot Standby PLC online in run mode?
Answer:
Yes, M580 HSBY CPU can be packed online in run mode.
But if it is a M580 stand alone CPU, we recommend to use Unity Pro v10 or later, as on Unity v8.1 there is an issue when online pack a running M580 CPU.
Is it possible to pack the memory of an M580 Hot Standby PLC online in run mode?
Answer:
Yes, M580 HSBY CPU can be packed online in run mode.
But if it is a M580 stand alone CPU, we recommend to use Unity Pro v10 or later, as on Unity v8.1 there is an issue when online pack a running M580 CPU.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.