Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you change the motor rotation on the ATV630 or ATV930 Process Drives?
Issue:
ATV630 or ATV930 Process Drives requires to change the motor rotation.

Product Line:
Altivar Process Drives

Environment
All

Cause:
Wants to change the motor's rotation

Resolution:
From the Main menu:
Select Complete settings
Select Motor parameter settings
Select Motor control
Select Output phase rotation
Factory default is ABC. This can be changed to ACB.