Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Connect and change parameters on a LXM32 drive using SoMachine
Issue:
Can I connect and change parameters on LXM32 servo drive using SoMachine?

Product Line:
SoMachine

Resolution:
In SoMachine, when you add a LXM32 drive to the network, you can double click it and go to the 'Configuration of the device' tab, where you can see a SoMove-like screen (See attached).
Just like the SoMove interface, you can connect to the drive and upload/download/edit parameters.

Schneider Electric Egypt and North East Africa

Attachment(s)
DTM.png [115.77 KB]