Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert 8.2 - If 'Reconfigure' is run on an upgraded Engineering Client/Secondary Server, it will fail on the 'Import System Key' leaving the server unusable

If an Engineering Client or a Secondary Server is upgraded to PME 8.2, and then subsequently, the installer is run in reconfigure mode, the reconfigure will fail at 'Import System Key'. When the this happens, the Engineering Client/Secondary Server will be rendered unusable. To recover, it is necessary to uninstall and reinstall PME.

1. It is recommended that Engineering Clients not be upgraded, but rather uninstalled, and then the new version of PME installed. If this is done, this problem can be avoided.

2. It is also possible to patch this problem by copying the attached file 'Security.Support.broker.xml' into the <INSTALL DIR>)\Schneider Electric\Power Monitoring Expert\Uninst_PowerMonitoringExpert\BrokerFragments folder, replacing the existing file. Once this is done, 'Reconfigure' will run correctly without errors.

Note that this is a problem with upgraded systems ONLY.

Schneider Electric Egypt and North East Africa

Attachment(s)
Security.Support.broker.zip [1.38 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: