How can we help you today?

It is not possible to installed on the same PC Unity Pro V11.1, V13.0 and V13.1 and the EFB Toolkit V8.0 or V8.1

Unity Pro V11.1 / V13.0 / V13.1 and Unity EFB Toolkit V8.0 or Unity EFB Toolkit V8.0 SP1 cannot be installed on same computer.
This will not be fixed in further release of EFB Toolkit.
For Control Expert V14.0 and gretaer version it is mandatory to install Unity EFB Toolkit V14.0
This information can be found inside the UP release note for Unity EFB Toolkit V8.0 but this is also true for Unity EFB Toolkit V8.0 SP1

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center