Issue:
Set up the ATV320 drive to run on a fan or pump application.
Product Line:
Altivar ATV320
Environment:
All
Cause:
Want to set up the ATV320 for fan and pump applications.
Resolution:
The ATV320 works well on variable torque and constant torque applications. The default is for common constant torque loads. A centrifugal pump and fan are variable torque loads. Set the Motor control type to V/F Quadratic.
Go to Conf -> FULL
Menu drC
Parameter Ctt, set to [V/F Quad.] (UFq): Variable torque. For pump and fan applications.
Set up the ATV320 drive to run on a fan or pump application.
Product Line:
Altivar ATV320
Environment:
All
Cause:
Want to set up the ATV320 for fan and pump applications.
Resolution:
The ATV320 works well on variable torque and constant torque applications. The default is for common constant torque loads. A centrifugal pump and fan are variable torque loads. Set the Motor control type to V/F Quadratic.
Go to Conf -> FULL
Menu drC
Parameter Ctt, set to [V/F Quad.] (UFq): Variable torque. For pump and fan applications.
Released for: Schneider Electric Egypt and North East Africa