Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the SER2408/3200 device to work with the Generator Performance module in PME.

Issue
When attempting to assign I/O in the generator performance module, one is unable to locate all input assignments.

Product Line

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024


Environment
Generator Performance Module


Cause
Before the device can be properly configured in the Generator Performance Configuration Tool it must first be configured and added into PME properly.
After device data is logged into the database, you can assign device measurements using the Generator Performance Configuration Tool with EPSS Test Module.

Resolution
Please refer to page 55 of the Generator Performance Configuraiton guide for instructions on configuring the SER hardware.

Schneider Electric Egypt and North East Africa

Attachment(s)
Generator Performance Guide.pdf [2.77 MB]