Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does ATV212 Remote Keypad (VW3A1101) switches to Frequency if screen not touched and goes dim, even though Custom RPM display has been set up?
Issue:
ATV212 Remote Keypad switches to Frequency even though Custom RPM display has been set up

Product Line:
ATV212

Environment:
All

Cause:
NA

Resolution:
This can happen if F702 =0 so need to set F702=60 for one pair of motor poles.