Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the blinking COM status led mean on the ATV630 and ATV930 Process drives?

Issue:
ATV630 and ATV930 Process drives with blinking COM status led.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
Com's status LED will blink when they connect the remote HMI display to the modbus port.

Resolution:
LED will flash when the fieldbus is active and communicating.

Schneider Electric Egypt and North East Africa