Issue:
Customer wants to transfer the ATVLogic programming between ATV320 Drives
Product line:
Altivar 320, ATV320
Environment:
all
Cause:
n/a
Resolution:
ATVLogic can be transferred using Multiloader (V3.17 and higher) and Simpleloader (V1.7 and higher). You should be able to successfully transfer all ATV320 programming, including ATVLogic.
To be successful you have to ensure the drive is stopped and that the FB Status (FbSt) is Stop:

If the FB status is Run, you must change FB Command (FbCd) to Stop.
Customer wants to transfer the ATVLogic programming between ATV320 Drives
Product line:
Altivar 320, ATV320
Environment:
all
Cause:
n/a
Resolution:
ATVLogic can be transferred using Multiloader (V3.17 and higher) and Simpleloader (V1.7 and higher). You should be able to successfully transfer all ATV320 programming, including ATVLogic.
To be successful you have to ensure the drive is stopped and that the FB Status (FbSt) is Stop:
If the FB status is Run, you must change FB Command (FbCd) to Stop.
Released for: Schneider Electric Egypt and North East Africa