Issue:
Wiring a potentiometer to an ATV320
Product Line:
Altivar 320, ATV320
Cause:
Wiring and installation
Resolution:
Using the +10V source of the drive, hook up to +10, AI1, and COM.
AI1 terminal is middle (wiper) connection for a potentiometer.
+10 is the drive's 10Vdc source.
COM is neutral.
Wiring a potentiometer to an ATV320
Product Line:
Altivar 320, ATV320
Cause:
Wiring and installation
Resolution:
Using the +10V source of the drive, hook up to +10, AI1, and COM.
AI1 terminal is middle (wiper) connection for a potentiometer.
+10 is the drive's 10Vdc source.
COM is neutral.
Released for: Schneider Electric Egypt and North East Africa