Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you connect the VW3A3616 Ethernet card to the ATV320 C suffix or compact version drive?
Issue:
Connect the VW3A3616 Ethernet card to the ATV320 compact version.

Product Line:
ATV320 with C suffix only

Environment:
All

Cause:
There is not a slot for the Ethernet card card to fit the ATV320 with C suffix.

Resolution:
The VW3A3616 card will not fit directly into the ATV320........ C  or compact version drive without the VW3A3600 add on option.
The VW3A3616 card will fit directly into the ATV320 ....... B or Book self version without the need of the VW3A3600 add on option.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV320_IS_Option_module_adapter_NVE22661_01.pdf [570.79 KB]