Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is PIF fault on an ATS48?
Issue:
How do you resolve the ATS48 tripping on PIF immediately at run command?

Product Line:
Altistart 48, ATS48

Environment:
All models

Cause:
NA

Resolution:
PIF is a phase inversion fault.
At each new run command, the ATS48 checks the line supply phase rotation.  This fault appears if the measured phase rotation on L1-L2-L3 does not match the setting for PHr in the PrO menu.  If the PHr is changed, cycle control power for the new setting to take effect.

Schneider Electric Egypt and North East Africa