Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the difference between Standard Data-Set and Legacy Data-Set ,in Modbus Communication NS,NT/NW ?
The standard data-set: is a global entity that collects the most useful information of each IMU module in one convenient table.
  • The benefit is that in one location there is up-to-date information with three read requests.
  • The standard data-set can be used with IFMv2 ,IFE or EIFE interface
  • The main information needed for remote supervision of a Compact NSX, Compact NS, Masterpact NT/NW or Masterpact MTZ circuit breaker is contained in the table of common registers starting at register 32000
  • The standard data-set is defined in the 32000 to 32435 register range.

The legacy data-set: is a global entity that collects the most useful information of each IMU module in one convenient table.
  • The benefit is that in one location there is up-to-date information with two read requests.
  • The legacy data-set can be used with IFM and IFE interface.
  • The main information needed for remote supervision of a Compact NSX, Compact NS, or Masterpact NT/NW circuit breaker is contained in the table of common registers starting at register 12000.
  • The legacy data-set is defined in the 12000 to12165 register range.
NOTE: The legacy data-set is compatible with previous versions of the Micrologic trip unit.