Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
DUP2 Does Schneider Electric offer the Berger Lahr EXRDM3913/50NEA motor or a suitable replacement?
No, the Berger Lahr EXRDM3913/50NEA motor with ID number 52951045500 is a special customized version for the company W&H.
This type is proprietary and is reserved for the company W & H and can not be purchased from Schneider Electric.
The customer must contact the OEM machine builder Windmuller & Holscher for a spare EXRDM3913/50NEA motor with ID number 52951045500.