Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How do I select the proper rated output (burden) value of my voltage transformer?

Sometimes one can select a relatively high value of rated output (burden) for a given voltage transformer as it is commonly thought the better choice when we are not sure about the typical burdens (loads) connected to our voltage transformer secondary.

IEC 61869-3 gives the standard values for rated output (burden) for a given voltage transformer:

image 1

image 2


In many cases where devices connected are mainly of micro-processor based protection /metering equipment, the overall burden can only be a few VAs; in other words a burden range (I) voltage transformer is considered adequate in many cases.

It is important to know that using an "oversized" voltage transformer rated output (burden) has a negative impact on accuracy thus increasing the error of the measurements.
The below highlights provides the limits of error which IEC 61869-3 specifies for each burden range.
image 3
image 4


Finally, it is important not to oversize your voltage transformer too far beyond the actual need for rated output in order to avoid increase of errors at a lower value of burden applied.