Issue:
Attempting to connect multiple devices to the Modbus RTU Port.
Product Line:
Altivar 212, ATV21, S-Flex
Environment:
All
Cause:
N/A
Resolution:
No.
The Modbus RTU RJ45 port is only designed to accept one path of signal over the network.
The drive can only have one master on one port.
Attempting to connect multiple devices to the Modbus RTU Port.
Product Line:
Altivar 212, ATV21, S-Flex
Environment:
All
Cause:
N/A
Resolution:
No.
The Modbus RTU RJ45 port is only designed to accept one path of signal over the network.
The drive can only have one master on one port.
Released for: Schneider Electric Egypt and North East Africa