Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the BMXPRA0100 comply with security notification SEVD-2017-048-02
Issue
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?

Product Line
BMXPRA0100

Environment
Windows 10

Resolution
Is the BMXPRA0100 compliant with security notification SEVD-2017-048-02?

Exec firmware version 2.9 is compliant with SEVD-2017-048-02.
Only PV version 12 and above is compliant.