Question:
What’s the difference between Harsh and Coated modules for Modicon PAC products?
Answer:
In terms of protection level for severe environments as well as characters , they are same.
The only difference lies in the operating temperature.
Harsh module works at -25 °C~70°C while Coated module works at -25°C~60°C or 0°C ~60°C.
Released for: Schneider Electric Egypt and North East Africa