Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for Lonworks communication card option for ATV212 drives?
Issue:
Lonworks communication card part number option for the ATV212 drives.

Product Line:
Altivar 212, S-Flex with ATV212

Environment:
All

Cause:
Option card

Resolution:
VW3A21212 is the Lonworks option card.

Lonworks

The ATV21 and ATV212 have different part numbers and option cards for them, and cannot be used interchangeably.
This provides a four-screw terminal block for connection to Lonworks network.  Install in place of standard control board that comes mounted in the Altivar 212 drive.
The I/O count is reduce to 3 logic inputs, 1 analog input and 1 NO/NC relay.

When this card VW3A21212 is installed the original control board is replaced and the original BACnet and Modbus communications are lost.
In case of an ATV212 S-Flex with LonWorks, the orginial control card with BacNet and Modbus is send together with the S-Flex, in case that the customer wants to go back with the original control card.

**Note: With this card installed, you have to write to this drive with Lonworks. You cannot monitor only.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center