How can we help you today?

What is the difference between the ABE7CPA31 and the ABE7CPA31E connection sub-base? Which of them can be used with the M340 BMXAMI0800 and BMXAMI0810 analog input modules connected to a HART device?

Comparing between ABE7CPA31 and ABE7CPA31E wiring diagrams the differences are:
  • The Telefast ABE7CPA31E there is a low pass filter for each channel for HART applications.
  • It is exclusively for current loop measurements with a 250 ohm shunt is present on each channel.








































  • But the Telefast ABE7CPA31 can be used with both Current and voltage sensors and can't be used in case HART information is part of the signal to be measured.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center