Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which version of LTU for Micrologic Compact NSX works with Windows XP, 7, 10?
LTU versions up to V9.2.2 supported Windows XP and Windows 7

From LTU V10.0.0, support for Windows 7 and 10 was added. However, Windows XP is no longer supported with this version.