Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How and where to use hardware kit HRB73195 that is supplied with PM5100/PM5300?
Issue:
The installation technician may be confused as to what the HRB73195 kit supplied with the PM 51XX/53XX is used for

Product:
PM5000 Series Meters

Environment:
Meter Installation

Resolution:
This is a Modbus RS-485 line terminating resistor and is only installed on the last meter of the daisy chain.


Schneider Electric Egypt and North East Africa

Attachment(s)
HRB73195_Hardware kit.JPG.jpg [1.77 MB]