Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ION 6200 be wired according to one of the 'Delta Direct' schematics, but left in the 'Delta' volts mode on the meter?
Issue:
A customer has an ION 6200 unit that is currently wired using one of the 'Delta' system type schematics, but the meter is revenue sealed and, in the interest of time to send the meter back for resealing, would like to jumper the Vb and V ref connections in order to line up with the 'Delta Direct' schematics.

Product Line:
ION 6200 series

Environment:
meter wiring

Resolution:
This wiring configuration can work with the caveat that the Delta volts mode is limited to reading 400 volts line to line max.  If higher voltage levels are applied the values may be clipped.