Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any relevance of computer clock time for Firmware upgrade of device using Ecoreach?
Yes, it is very relevant. Because, while doing the firmware upgrade of the device within smart panel using Ecoreach, Ecoreach validates the integrity of the Signature file (packaged inside the firmware binary file). And if the computer Clock time is dated back to an older date (like before to 2016), the firmware upgrade of the device will fail.

Schneider Electric Egypt and North East Africa