How can we help you today?

PlantStruxure PES [V4.1]: How to setup AS-I (Actuator Sensor Interface) Device communication with M340 Controller using PES

Goals and Symptoms

The purpose of this document is to provide step by configuration for integrating AS-I device with M340 using PES.

Facts and Changes

This document has been created for PES version 4.1, however it can be used for other later version as well.

Causes and Fixes

The integration of AS-I device is not fully supported by PES using its Application Interface. However you can configure AS-I Device using Control Participant Tool (Unity Pro) and then you can map these AS-I device variable to PES variables.

This document help PES users to manage and integrate AS-I based devices into PES using control participant tool and explains the step by step procedure to map it to PES application instances.

Schneider Electric Egypt and North East Africa

Attachment(s)
ASI with M340 Controller using PES.pdf [490.25 KB]
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
  • Help and Contact Center