How can we help you today?

The correct Ambient air temperature of BMXPRA0100 is "-25...70 °C" or "0...60 °C"?

Question:
In BMXPRA0100's datasheet, the operating ambient air temperature is -25...70 °C.
But on the side of the module it say 60°C.
Who is right?

Answer:

The correct operating ambient air temperature of BMXPRA0100 is 0...60 °C, the datasheet is wrong.

Schneider Electric Egypt and North East Africa

Attachment(s)
Modicon X80 I_Os_BMXPRA0100.pdf [70.54 KB]