Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the motor current ratings for the ATV680 low harmonic 600 hp and 700 hp drives?
Issue:
Motor current ratings for the ATV680 low harmonic 600 hp and 700 hp drives

Product Line:
ATV680

Environment:
All

Cause:
Motor current ratings not listed in the manual.

Resolution:
The ATV680C40Q4X1 = 600HP 730 amps
The ATV680C50Q4X1 is 700HP 900 amps

The attached document shows the ATV680 being available up to 800KW but you can only get this unit for now up to 700HP normal duty.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV680 current ratings up to 700HP max size.pdf [78.52 KB]