Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Analog Output power supply be deactivated to connect to an externally powered monitor device on altivar process drive?
Issue:
Can the Analog Output power supply be deactivated to connect to an externally powered monitor device on altivar process drive?

Product line:
Altivar Process, ATV600 ATV900

Environment:
All

Cause:
Needs to use an external power supply

Resolution:
The Altivar Process drives do not have a means to deactivate the power supply on the AQ1 or AQ2 terminals.  The customer will need to find an external device to convert the signal.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center