Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What alarms are available in PM3200 series meters?

Issue

What alarms are available in PM3200 series meters?

Product Line

PowerLogic PM3200 Series

Environment

PM3200 Series Energy Meters – Alarm Features

Resolution

The PM3200 series meters provide setpoint-driven alarms. These alarms can be configured based on user-defined thresholds for various electrical parameters.

Available alarms include:


1