Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many tariffs are available in PM3255 ?

Product Line

PM3255

Environment

Installation and commissioning.

Resolution

The power meter provides multi-tariff energy accumulation. It supports up to 4 tariffs.
The tariff switching has the following 3 kinds of control modes:
• Digital input
• Communication
• Internal real-time clock (RTC)

Schneider Electric Egypt and North East Africa