Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I connect a XML Client to OFS V3.6?
After configuring COM / DCOM and IIS as specified in the User Manual, the user must add 2 more STEPS

Step 1: In “Internet Information Service (IIS)”  Add “Windows Authentication”
Access path:
Control Panel\All Control Panel Items\Programs and Features
Click in “Turn windows facture ON or OFF”
Select “Internet Information Service (IIS)” \World wide Web Services\Security
Select “Windows Authentication”

Step2:
Internet Information Services configuration on Windows x64 platforms
On x64 platforms, the IIS OFS application pool must have the property Enable 32-Bit applications set to TRUE.

Schneider Electric Egypt and North East Africa