Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between Compensated and Non Compensated trip units ?
The circuit-breakers with non compensated thermal tripping elements have a tripping current level that depends on the surrounding temperature. When the temperature in which the CB is located exceeds its reference temperature, it will therefore be “derated”.

While,for compensated thermal-magnetic tripping units,they include a bi-metal compensating strip which allows the overload trip-current setting (Ir or Irth) to be adjusted, within a specified range, irrespective of the ambient temperature.