Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the MTBF for the M580 SFP socket 490NAC0100?
The MTBF values are in hours for 490NAC0100 as shown below
MTBF 30° ContinuousMTBF 30° IntermittentMTBF 60° ContinuousMTBF 60° Intermittent
13 386 3285 767 1528 620 0004 783 955