Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Schneider MBX Driver 8.1 compliant with Windows 10?
The Schneider MBX Driver 8.1 is not compliant with Windows 10 but it is possible changing registry keys to make it. Please follow procedure as describe inside the PDF file ; note that must be done before to install the Schneider MBX Driver 8.1.

Schneider Electric Egypt and North East Africa

Attachment(s)
WIndows 10 MBX Driver Suite Procedure.pdf [559.02 KB]