Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are temperature settings required for "T" type thermal protection on Trihal dry type transformers?
The transformer rating plate shows temperature rise class "F", which requires the user to apply setting of the T digital thermometer/controller with a maximum temperatures of:
  • 140°C for "alarm 1" and,
  • 150°C for "alarm 2".

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: