Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the firmware flash cable used on the ATV320 Drives?
Issue:
Part number request for the firmware flash cable used on ATV320

Product Line:
VW3A8122

Environment:
All

Cause:
Flash cable used to update the firmware

Resolution:
The VW3A8122 cable is the flash cable used for updating the firmware on the ATV320 Drive.

Schneider Electric Egypt and North East Africa

Attachment(s)
Altivar Machine ATV320 flashing tool (1).pdf [205.19 KB]