Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Dashboard functionality breaks after an in-place upgrade from Power Monitoring Expert 8.1 to 8.2 (if Azzo gadgets are installed)
Issue
After an in-place upgrade from PME 8.1 to 8.2, Dashboards will stop working if Azzo gadgets are installed.

Product Line
Power Monitoring Expert 8.1/8.2

Environment
PME Dashboards

Cause

Prerequisite system/steps:

8.1 platform files placed in dashboards

\

bin & slideshow

\

bin via msi as they were not

there in this version;

a.

b.

Dashboards and AZZO gadgets function at this stage;

1.

PME 8.1 with any AZZO gadgets installed;

We have seen instances where the 8.2 installer has not placed new files in the

folder. We noticed that ProductInfo.xml pointing to PME 8.1 causing 2.b below to

fail. This could likely be due to existence of files linked to different msi. If this is

true than step 3 and 4 should uninstall existing files from Dashboards, slideshows

\

bin and place them from system

\

bin.

We have to be prudent with this issue and observe it on individual upgrades. At

least few upcoming ones.

a.

The 8.2 installer places these same platform files in these same folders now;

b.

Dashboards 'should' function at this stage;

2.

Upgrade to PME 8.2;

This will most likely remove platform files from these location (msi reference counting

may cause this to sometimes be different);

a.

b.

Dashboards will most likely be broken at this stage;

3.

Uninstall AZZO 8.1 gadgets;

i.

If the platform files exist, they will not be overwritten;

ii.

If the platform files no not exist, they will be copied from the system

\

bin

iii.

The above is intended to handle both the new install case and upgrade case;

iv.

Dashboards & AZZO Gadgets should function in this case;

a.

Using the new installer package:

Platform files were to be installed via the AZZO msi and given these were also

installed by the PME installer the outcome is likely to be inconsistent as we have

seen.

i.

ii.

Dashboards are likely broken in this case;

Prerequisite system/steps:

8.1 platform files placed in dashboards

\

bin & slideshow

\

bin via msi as they were not

there in this version;

a.

b.

Dashboards and AZZO gadgets function at this stage;

1.

PME 8.1 with any AZZO gadgets installed;

We have seen instances where the 8.2 installer has not placed new files in the

folder. We noticed that ProductInfo.xml pointing to PME 8.1 causing 2.b below to

fail. This could likely be due to existence of files linked to different msi. If this is

true than step 3 and 4 should uninstall existing files from Dashboards, slideshows

\

bin and place them from system

\

bin.

We have to be prudent with this issue and observe it on individual upgrades. At

least few upcoming ones.

a.

The 8.2 installer places these same platform files in these same folders now;

b.

Dashboards 'should' function at this stage;

2.

Upgrade to PME 8.2;

This will most likely remove platform files from these location (msi reference counting

may cause this to sometimes be different);

a.

b.

Dashboards will most likely be broken at this stage;

3.

Uninstall AZZO 8.1 gadgets;

i.

If the platform files exist, they will not be overwritten;

ii.

If the platform files no not exist, they will be copied from the system

\

bin

iii.

The above is intended to handle both the new install case and upgrade case;

iv.

Dashboards & AZZO Gadgets should function in this case;

a.

Using the new installer package:

Platform files were to be installed via the AZZO msi and given these were also

installed by the PME installer the outcome is likely to be inconsistent as we have

seen.

i.

ii.

Dashboards are likely broken in this case;


After an upgrade, specific files may be missing from the dashboards\bin and slideshow\bin folder.

Resolution
This issue has been corrected in the latest install package for the Azzo Xpert System Diagnostics.

Uninstalling the existing Azzo diagnostics package and installing the latest 8.2 diagnostics package from the link below should resolve the issue. This is the recommended solution.

https://www.dropbox.com/s/g4nfpxaarvudpyw/Xpert System Diagnostics Trial 8.2.exe?dl=0
NOTE: To uninstall the existing Azzo diagnostics package, re-run the previous installer used to install the package and select the Remove option once prompted.

To manually correct this issue, simply ensure the following files exist in the dashboards\bin and slideshow\bin folder. (You can copy them from another bin folder in the system)
- Configuration.dat
- Gadget.Data.dll
- Internationalization.dll
- Interop.Internationalization.dll
- LicenseManager.Logic.dll
- Licensing.LicenseManager.dll
- ProductInfo.xml
- SELMBrick.dll