How can we help you today?

PlantStruxure PES [V4.2]: Dealing with unresponsive Genies above AN 9999 in PES 4.1 and PES 4.2.

Goals and Symptoms

How to correct the Genies inside PES Vijeo Citect having Animation Number more than 9999 which will not respond for any action during Citect runtime.

Causes and Fixes

The attached document illustrates the available methods to correct unresponsive Genie issue.The procedurre details to correct this issue using Citect patches inside PES VM. The patch replaces citect.frm inside VM Citect to accept the AN's more tha 9999.

Schneider Electric Egypt and North East Africa

Attachment(s)
VJC AN9999 Patch PES 42.zip [24.64 KB]
VJC AN9999 Patch PES 41.zip [24.32 KB]
PES 4142 VJC AN MORE THAN 9999 Fix.pdf [1.41 MB]