Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you change the PRT power identify ratings on the ATV630 drive like the ATV61 drives?


Cause:
Wants to change the HP size in the field like the old ATV61 PTR parameter settings.

Resolution:
If you change the power board, you will get prompted to choose.

However, the standard drive does not have the same IP00 and IP20 settings like the ATV61 unless you are
Trained Field Services and have access to special access to the services tab in Somove..

So normally no it's not a standard setting in the drive.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)