Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there status words available which will allow me to see module health on the ERIO network?
Issue:
Are there status words available which will allow me to see module health on the ERIO network?
Product Line:
ERIO network, Quantum, Modicon
Resolution:
Yes, the following System Words will provide the health status of each IO module on the ERIO network.


%SW641-702   Referred to as ERIO Module Health (refer to Unity Help for detail as to which words apply)
16 bits of the word represent the 16 potential slots in a Quantum backplane.
0 = unhealthy or not mapped
1 = healthy module.

R-2192018

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)