Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you set the timeout settings on the ATV71 drive using IO scanner and Ethernet TCP-IP?
Issue:
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP

Product Line:
ATV71

Environment:
All

Cause:
Loss of communications from the Ethernet.

Resolution:

If the customer needs to change the time out for Ethernet communications he can do it from the web page  or the (Tout) parameter in the drive.

The default is 2 seconds.

See the attachment.

Schneider Electric Egypt and North East Africa

Attachment(s)
Ethernet timeout settings on webpage.jpg [115.12 KB]