Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Efficiency of the EV Link Chargers?
1) Inside EV Link a mother board with a 24V power supply commanding a contact is installed.
2) Less than 100W of consumption when the CT is closed. We are just a gate between the grid and the car.

So the maximum consumption is 100w (dedicated to 24v power supply, motherboard, contactor and led). Efficiency will be,
If the load is a 3,7kW (16A 1P) efficiency = 97%
If the load is a 22kW (32A 3P) efficiency = 99,5%

But, also consider the Harmonics, Power factor produced by the Car itself which will affect efficiency.