Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
B10d calculation for normally closed contact ZBE102 ?
FOR NORMALLY CLOSED CONTACT (ZBE102)
The fault exclusion described in Table D8 from ISO 13849-2 2012 can be considered
As our contact ZBE102 respects requirements and verification test according to the IEC 60947-5-1:2003 Annex K “Special requirements for control switches with direct opening action”, so the B10d cannot have to be considered thanks to the exclusion fault.

Schneider Electric Egypt and North East Africa

Attachment(s)
17-017 C&S B10d for ZBE102.pdf [218.36 KB]
ISO 13849-2 2012 Table D8.docx [150.26 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: