Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the wiring diagram of serial RS232 programming cable for Scadapack 350E RTU ?

This cable is used to connect from an RJ-45-based RS-232 port on the RTU to a DE-9S connector on DTE such as a PC. A 3 m (10 ft.) long cable is available from Schneider Electric using part number TBUM297217.

RJ-45 to DE-9S DTE cable Description

RJ-45
8 Pins

SCADAPack DTE Function

DE-9S DTE Function

DE-9S

Shield connects to shell

6

TxD

RxD

2

5

RxD

TxD

3

4

GND

GND

5

1, 2, 3, 7 and 8 are not connected at this end.

Wires not connected at this end.