This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
RJ-45 to SCADAPack Vision
This cable is used to connect from the COM3 (RJ-45-based RS-232) port on the RTU to a DE-9S connector on a SCADAPack Vision. A 1.5 m (5 ft.) long cable is available from Schneider Electric using part number TBUM297237.
RJ-45 to SCADAPack Vision cable Description
| RJ-45 | SCADAPack E Function | SCADAPack Vision Function | DE-9S |
| Shield connects to shell | |||
| 6 | TxD | RxD | 2 |
| 5 | RxD | TxD | 3 |
| 4 | GND | GND | 5 |
| 3 | DTR / Test 2 | ON switch | 1 |
| 2 | DCD / Test 1 | ON switch | 4 |
| 1 | +5 Vdc Out | +5 Vdc In | 9 |
| 7 and 8 are not connected at this end. | Wires not connected at this end. |
Released for: Schneider Electric Egypt and North East Africa