Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which version of Unity Help instructions to reference when configuring IP Secure (IPsec) in Windows 7 for communications to a BMENOC0301/0311?
Issue
This resolution describes which version of Unity Help instructions to reference when configuring IPsec in Windows 7 for communications to a BMENOC0301 or BMENOC0311.  Unity Pro v13 Help contains instructions for configuring IPsec in Windows 7 for new encryption algorithms that are not yet released in the BMENOC0301/0311 firmware.  This resolution clarifies which version of Unity Pro Help instructions to reference when using specific firmware versions.

Listed below are the BMENOC0301 and BMENOC0311 firmware versions.  Each version contains the IPsec encryption algorithms that are implemented in each and the correct Unity Pro Help version to configure IPsec.


Product Line
Unity Pro V8.1
Unity Pro V12
Unity Pro V13
BMENOC0301
BMENOC0311


Environment
Windows 7


Resolution
For BMENOC03x1 firmware version 2.09
  • IPsec uses SHA-1 and 3DES encryption algorithms.
  • Configuration instructions for SHA-1 and 3DES algorithms are found in Unity Pro 12 Help, ‘Configuring IP Secure Communications’ for Windows 7.
  • Use Unity Pro v8.1 Plantstruxure Library with DTM versions v3.6.x (and later) to run IPsec.

For BMENOC03x1 firmware version 2.10
  • IPsec uses SHA-1 and 3DES encryption algorithms.
  • Configuration instructions for SHA-1 and 3DES algorithms are found in Unity Pro 12 Help, ‘Configuring IP Secure Communications’ for Windows 7.
  • Use Unity Pro v8.1 Plantstruxure Library with DTM versions v3.6.x (and later) to run IPsec.

Unity Pro v13 Help contains instructions for configuring IPsec in Windows 7 for encryption algorithms SHA-256 and AES-128-CBC, which will be implemented in firmware release v2.11

For firmware version 2.11
  • IPsec will use SHA-256 and AES-128-CBC encryption algorithms.
  • Configuration instructions for SHA-256 and AES-128-CBC algorithms are found in Unity Pro 13 Help, ‘Configuring IP Secure Communications’ for Windows 7
  • Use Unity Pro v12 PlantStruxure Library with DTM versions v3.8.x (and later) to run IPsec.
    Summary
BMENOC0301
BMENOC0311
FW Version
IP Secure Encryption AlgorithmsIPsec Configuration Help
found in Unity Pro Version
2.09SHA-1, 3DES12
2.10SHA-1, 3DES12
2.11SHA-256, AES-128-CBC13 and greater